Part Number: RF430FRL153H
Other Parts Discussed in Thread: RF430FRL152H, RF430FRL154H, RF430FRL152HEVM, DLP-7970ABP, TRF7970A, MSP-FET, PCA9306
Hello,
I intend to use the RF430FRL153H for a project. I need to read an analog sensor and, after the reading, send an 1.5 V signal to reset the sensor.
So the sensor output pin would be connected to the ADC, and I would like to send the reset signal using a GPIO.
My question is whether I need a custom firmware for this or I could use the built-in ROM functions.
Thanks.