Other Parts Discussed in Thread: CC2530, CC2530EM, CC1100, CC2500, CC2511, CC2531, CC2530EMK
Hello Everyone:
I'm having some trouble with the CC2530 SoC. Here is the explanation:
I made my own “Development Kit” by copying the schematic in the datasheet of the cc2530, the application circuit in page 22. I just connect the digital ports and the reset to external pins in order to have access to them and be able to run some tests, the voltage and GND pins are connected as shown in the schematic as well as the other passive components and crystal.
I have the CC Debugger and I connect it to the SoC as the User’s Guide says, I mean I connect the CC Debugger directly to the SoC with no Development Kit, but the CC debugger is not recognizing the SoC (The LED In the debugger is RED all the time).
I read other answers in this same forum and they indicate some solutions like Pull ups resistors and capacitors, I have tried all of them but the CC Debugger is still not recognizing the cc2530.
The question is: Is there any other component or configuration or schematic needed to program the SoC with the CCDebugger.
I will appreciate all the help, because I am kind of stuck.
Thank you