Part Number: CC2652R
Other Parts Discussed in Thread: CC2592, CC2590, CC1352P, , CC2650, CC1352R, Z-STACK
Hello,
Is there any RF booster for CC2652?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Have you looked into CC2590/ CC2592?
Or CC1352P which cover 2.4 GHz and has a built-in 20 dBm PA?
Dear Yikai,
RF Booster as in CC2592 as mentioned by @TER.
But can CC2592 be directly interfaced with CC2652? and does the CC2652 SDK have support for CC2592?
Yes, CC2592 can be interfaced to CC2652R. However, I would suggest you to use CC1352P as it is also suggested by TER already.
Dear Yikai,
Thank you for the suggestion, I will consider CC1352.
But can you just calirfy, if the CC2652 SDK has support for CC2592?
Please note it’s CC1352P which embeds PA not CC1352R. As I know, current SDK doesn’t include CC2592 support but you can add it like supporting CC2592 to CC2650 in Z-Stack Home 1.2.2a.
Dear Yikai,
Thank you. Will look into this and get back to you if I face problem with integration.