Other Parts Discussed in Thread: CC1310
I am facing an issue with CC1312R1 where the Event_post() fails to trigger at all.
Below is my code snippet where the device basically waits for the ACK over the UART and then should do an event post depending on the ACK/ No ACK.
After debugging and checking the signals, the CC1312 is actually getting the ACK from the device and then prints out
LOG_INFO("UART_RXED_ACK from Modem!\n");
However, it then fails to do Event_post() at all.
if (PCMD_Data.dvmn_AckNckEpoch.ACKorNCK == 1)
{//If ACK: Event_post RX'ed_ACK
LOG_INFO("UART_RXED_ACK from Modem!\n");
Event_post(UartOperationEventHandle, UART_RXED_ACK);
}
else
{//If NACK: Evenet_post RX'ed_NACK
LOG_DBG("UART_RXED_NACK!\n");
Event_post(UartOperationEventHandle, UART_RXED_NACK);
}
I have previously tested this piece of code on CC1310 where everything works as expected but after implementing the same in CC1312R1, it is not working.
Am I missing anything that's why it is not triggering the event post?
Other declarations are as follows to handle the event
static Event_Handle UartOperationEventHandle; #define UART_RXED_ACK (uint32_t)(1 << 4) #define UART_RXED_NACK (uint32_t)(1 << 5)