This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: Frequency Hopping for FCC 15.247(a)

Part Number: CC1352R
Other Parts Discussed in Thread: , SYSCONFIG

Hello,

 I have a question regarding example code for FCC 15.247(a) testing for sub 1-GHz testing for my product which uses the CC1352R. Do you have example code available that would allow my device to do the random channel hopping operations? Is it possible to achieve the channel hopping without the device communicating with another device?

I was reviewing the FCC test report for the LPSTK-CC1352R (see link below) and the test setup for sections 3.1-3.3 show the device just connected to a spectrum analyzer. This would imply that the device was set up to randomly hop without needing to communicate with another device.

https://fccid.io/Z64-LPSTKCC1352R/Test-Report/Test-Report-DSS-4502030

If another device is required for channel hopping, can you point me to example code that would allow me to do this?

Thanks,

Braydon