This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: How to get bit error rate (BER) and packet error rate (PER) on the 1310?

Part Number: LAUNCHXL-CC1310


On the 1310, how can I get the radio link strength information, such as bit error rate and packet error rate?

  • The relationship between BER and PER is given by: https://en.wikipedia.org/wiki/Bit_error_rate meaning that BER is possible to calculate based on PER.

    PER is easily measured: You send x packets and check how many you receive. Ideally this should be done using a signal gnerator as source and doing a test where the input level is increased in 1 dB step to get a PER vs level curve. For a input signal ~3 dB above the sensitivity limit and above, the PER should be 0 % until the saturation limit.