Hello,
In CC2511 datasheet it is one application circuit that uses 3rd Overtone crystal oscillator. It uses some extra inductance and capacitor.
My question: is it possible to use 3rd overtone and have USB and RF?
I have one like this. I've placed the capacitors and inductance as in datadheet. It is seen as HS RCOSC and not as XOSC
The frequency is as defined in datasheet Fref = 48Mhz/2;
CLKSPD is forced to 1 because CLKCON.OSC=1 so the system frequency wil be Fref/2 => 12MHz
I've set-up the serial channel for 9600 baud based on this calculation and it works (also the timer looks ok)
Can I use USB in this case?
I've read that USB cannot be used with HS RCOSC. I'm not a specialist in Crystals but I was expecting that 3rd Overtone can be used instead of a fundamental crystal. Am I mistaking?
Thanks'
Can someone tell me if this one CFPS-39 can be used with cc2511?