This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: Pattern Recognition

Part Number: CC1200


Hi Folks,

I am replacing  XE1203 Transceiver Radio to CC1200 radio,

We have had one Pattern recognition block in XE1203.

"This feature can be activated by setting RTParam_Pattern to high while in receiver mode. The incoming NRZ bit
stream is compared with a pattern stored in PATParam_Pattern registers. The PATTERN output is driven by the
output of this comparator and is synchronized by DCLK. It is set to high when a matching condition is detected,
otherwise set to low. PATTERN output is updated at the rising edge of DCLK. The number of bits used for
comparison is defined in the ADParam_Psize register and the number of tolerated errors for the pattern recognition is
defined in the ADParam_Ptol register. The next figure shows the pattern matching operation"

Do we have a similar feature available in the CC1200 Chip set?

Or shall we bypass this pin in our new design.

Thanks