Hi,
I'm starting a new project for a client that needs a 433 MHz transmitter and receiver. The distance between the 2 communicating devices will be fixed at approximately 5 ft apart. There will be potential obstructions of metal between the 2 devices. The data to communicate is 1-way only, and is just the value of a switch (open or closed).
Can you recommend hardware and firmware (including starting example code) that can handle this requirement?
Is there an existing firmware protocol stack for something like this? I need to understand the firmware effort required.
Thanks...
Brian