Hi,
When loading Custom Frequency Modulations into the CC1125. We are finding that intermediate frequency shifts are being removed by the CC1125 when transmitting. We push it in so as to slope towards the peaks instead of going straight from zero to the deviation, but when its transmitted from the 1125, its going straight from the carrier to the deviations, and ignoring intermediates.
What registers/things should I look for to get the CC1125 to pay attention to the intermediate frequencies, the main reason for doing CFM in the first place is because the standard Gaussian Filter doesn't shape the band well enough.