Looking for some help here to understand why we do not achieve the -123dbm sensitivity (for 1.2kHz data rate)

We have a UHF front end chain NF with the below parameters:
Freq Range = 400-450MHz
NF = 3.2dB (including CC1125)
Modulation = 2-GFSK
SNR Requirement = 12dB
Channel Filter = 10kHz
Using the above we should be in the region of -121dBm sensitivity from calculations. In reality (testing our hardware) we are getting -115dBm. Is there anything else I should consider before I look at possible inference in the system?