Hi,
I am configuring sniff mode in my application since i need to reduce my current consumption. I followed the excel sheet provided in this link (http://www.ti.com/lit/zip/swra428).
From this i understood that, major part of current consumption depends on the no. of preamble bytes . so on my receiver side i have configured the number of preambles as 30 since it consumes least current. although my transmitter is configured for 8bytes. When i measured the current on my RF board, i am observing that the current is ~8.2mA in all cases, irrespective of the preamble size configured on the RX size and i measured the current when there is no RF transaction. So my understanding is that, when the receiver is not receiving anything, the current consumption should be ~1.8mA when configured for 30 bytes preamble.
can you help me understand the scenario?
| PQT Termination Bit rate: 19200kbps, Osc Freq:40MHz |
||
| No of preamble | Expected Current consumption | Actual Current consumption |
| 8 | 8.260 mA | 8.260 mA |
| 24 | 2.306 mA | 8.260 mA |
| 30 | 1.814 mA | 8.260 mA |