This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: band support of 1076~1315

Part Number: CC1312R


Hi, 

Could you support a RF setting for the band of 1076~1315MHz. The DS show the band is supported but not CZed. the deal is okay. 

but when I tried to calculate the setting in the SRF studio, (2.24, latest version), but it return error. can't do the Packet TX-RX transmit. 

below is the PHY needs: 

Clip: CC1312R or CC1311R

Freq: 1076MHz - 1315MHz

Symbol rate:680K bps 、1M bps、2M bps.

Error correction :CRC

Modulation kernel: GFSK

preamble 4bytes,syncword 4bytes,playload 200bytes,CRC 2bytes

BR. Albin