Dear TI,
I have a time stamp application, but would like to use the 32Khz clock (SCLK_LF) as the clock source for the ticks since it will still be running in standby mode. Can I change the clock source of the time stamp module from the system clock to the SCLK_LF? I expect the RTC is being clocked by the SCLK_LF, but don't see an easy way to read the RTC ticks? I see I can create a clock from the ClockModule, but those all seem to use the system clock as their source as does the time stamp module.
Thanks,
Brett