This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC1352P7: HW design questions

Expert 4021 points
Part Number: LP-CC1352P7
Other Parts Discussed in Thread: CC1352P7

Hi,

We follow the LP's design and have few questions:

Q1 – We intend to operate Wisun in 868/915MHz @ 20dm power. Do we still need to mount the RF front-end matching circuit for 2.4GHz +5dBm and 868/915 +14dBm circuit and the RF switch?

Q2 – We couldn't find the specs of the Y2 crystal, please share with us.

Q3 – We are not implementing Bluetooth or RTC function. So for Wisun 868/915MHz communication only, do we need the 32.768KHz crystal in the design? 

Q4 – CC1352P7 support CJTAG, the signal from XDS110 debugger connected to CC1352P7 are:

  • WMCU_TMS
  • WMCU_TCK
  • WMCU_RESET

Are these above signals enough to do firmware download and code debugging?

Regards,

Kien Nguyen