Hi all,
We've been using CC1312 for some time and it's a great chip. Now I have a simple question - is there any way for the CC1312 to operate in the frequency band of about 71 - 88 MHz? And use a proprietary protocol with FSK modulation. For example, is there an undocumented function that will allow this? Or would this be achieved, for example, by reducing the frequency of the external crystal oscillator from 48MHz to 24MHz? Or some other way?
I will be happy for any advice.
Best regards
Frantisek Lysy