Hi Sub 1 GHz team,
I have a few questions about SWRA730, related to LAUNCHXL-CC1352P-4.
In SWRA730, section 1, it refers to figure 1-1 for a 433 to 510 MHz antenna. It recommends changing L4 to 19 mm for 868 to 930 MHz. I believe this refers to all 3 "horizontal" lengths being shortened to 19 mm, not just the bottom one. This works out to approximately 83 mm depending on how you measure total length, so about a 1/4 wavelength for the middle of the range. Is that right?
In section 5.5 of the same document, is it based on an antenna with L4=19mm, like I just described?
If the customer uses 0402 components instead of 0201, what concerns or advice would you have?
Thanks,
Darren