This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Does SDK version from 5.20.00.52 to 6.10.00.29 will help improve receiver strength?

Part Number: CC1352P

Hi Team,

Does SDK version from 5.2 to 6.10.00.29 will help improve receiver strength?

Background:

Self-built board with SDK 5.20.00.52 tested show lower receiver strength than the standard EVM board.

When using EVM Smart RF configuration transmission to self-built board, self-built board now could have the same strength. We assume that using upgrade SDK may help with issue. Thanks for the help.

Best Regards,

Tess Chen

  • Have you compared the RF settings (when doing a code export from SmartRF Studio) and the settings you are using when using SDK 5.20? 

    If you using the last SDK the settings used should be the same as used in the latest SDK. You can compare the settings you are using  to verify. 

  • We have compared the settings between the demo studio codes and SDK5.20. In demo studio codes and SDK, we just can look out 3 commands about RF setting.
    Are there any RF settings which we cannot discover?

  • Hi Tess,

    Can you give some more detail on how you are testing? E.g. which SDK example are you using for the SDK test? Which board are you using? How are you reading the sensitivity value?

    Cheers,

    Marie H