This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1312R1: XDS110 error

Part Number: LAUNCHXL-CC1312R1
Other Parts Discussed in Thread: UNIFLASH

Hi Team,

Our customer encounters an error when connecting this device.

Error initializing emulator:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
(Emulation package 9.7.0.00213)

I understand that this EVM as an emulator has a built in XDS110. I advised the customer to check the Host connection error however, it does not help.

Can you help debugging the error? The customer is using  CCS 11.2 on ubuntu 20.01

Thank you.

Regards