This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: dmm 154 sensor remote display LPSTK doesn't build

Part Number: CC1352R
Other Parts Discussed in Thread: SYSBIOS

Hello,

So I've somewhat resolved the xdc question by reinstalling the SDK, but now I have actual build issues and it looks like the included package repositories for xdc are actually incorrect:

You can see from this screen grab here that the first XDCPath entry has a garbled formatting which causes CCS to declare it as an invalid include path:

I manually edited this and it doesn't seem to help.

On a clean build there's errors for no rule to make target "build-xxxxxxxxxx" which seem to be automatically generated build targets and not related to any real errors.

If I rebuild without cleaning I can get a bit further but encounter this error:

#10008-D cannot find file "/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/apps/common/tirtos/src/sysbios/rom_sysbios.am4f"

In addition there's numerous undefined reference to ti_sysbios_family_armcc26xx type errors. 

Has anyone actually built this application in this release and gotten it to successfully compile? Please advise on how to get this building again.

Munan

  • Hi Munan,

    If you do not make any modifications to the example, does it build successfully? (warnings are allowed)

    Do you experience warnings like below:

    If you do, these warnings can be ignored, and you should not make any modifications to the XDCpath Package Repositories. See https://sir.ext.ti.com/jira/browse/EXT_EP-10830

    Regards,
    Nikolaj

  • Hi Nikolaj,

    I still get the same build error with a project that's imported directly from the SDK and built with no modifications. I tried both the ccs compiler and the ticlang just to be sure but the error is the same in both. 

    Munan

  • HI Munan,

    Can you share the entire build log of the unmodified example imported from the SDK?
    Is this only an issue for this specific example, or are you experiencing the same issue if you try to import other examples?

    Regards,
    Nikolaj

  • Hi Nikolaj,

    From a clean build:

    **** Clean-only build of configuration Release for project dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang ****
    
    /Applications/ti/ccs1120/ccs/utils/bin/gmake -k -j 9 clean -O 
    
     
    
    rm -rf  "syscfg/ti_ble_config.h" "syscfg/ti_154stack_config.h" "syscfg/ti_154stack_features.h" "syscfg/ti_dmm_application_policy.h" "syscfg/ti_dmm_custom_activities.h" "syscfg/ti_radio_config.h" "syscfg/ti_drivers_config.h" "syscfg/ti_utils_build_linker.cmd.genlibs" "syscfg/syscfg_c.rov.xs" "syscfg/ti_utils_runtime_model.gv" "syscfg/ti_utils_runtime_Makefile"  "../src/makefile.libs" "dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang.hex"  "configPkg/linker.cmd" "configPkg/compiler.opt" "syscfg/ti_ble_config.c" "syscfg/ti_build_config.opt" "syscfg/ti_ble_app_config.opt" "syscfg/ti_dmm_application_policy.c" "syscfg/ti_devices_config.c" "syscfg/ti_radio_config.c" "syscfg/ti_drivers_config.c"  "dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang.out" 
    
    rm -rf "syscfg/ti_ble_config.o" "syscfg/ti_dmm_application_policy.o" "syscfg/ti_devices_config.o" "syscfg/ti_radio_config.o" "syscfg/ti_drivers_config.o" "OAD/bim_util.o" "OAD/crc32.o" "OAD/flash_interface_ext_rtos_NVS.o" "OAD/mark_switch_factory_img.o" "OAD/oad.o" "OAD/oad_image_header_app.o" "OAD/oad_util.o" "application/ble_remote_display/remote_display.o" "application/ble_remote_display/startup/ble_user_config_stack.o" "application/ble_remote_display/startup/osal_icall_ble.o" "application/ble_remote_display/startup/rom_init.o" "application/ble_remote_display/util/util.o" "application/cui/cui.o" "application/lpstk/adxl362/scif.o" "application/lpstk/adxl362/scif_framework.o" "application/lpstk/adxl362/scif_osal_tirtos.o" "application/lpstk/lpstk.o" "application/lpstk/lpstk_sensors.o" "application/main.o" "application/sensor/link_controller/jdllc.o" "application/sensor/sensor.o" "application/sensor/ssf.o" "application/sensor/util/mac_util.o" "application/sensor/util/util_timer.o" "dmm/application_policy/dmm_priority_ble_154sensor.o" 
    
    rm -rf "drivers/nv/crc.o" "drivers/nv/nvocmp.o" "sail/hdc2010.o" "sail/opt3001.o" "software_stacks/ble_stack/icall/icall.o" "software_stacks/ble_stack/icall/icall_cc2650.o" "software_stacks/ble_stack/icall/icall_user_config.o" "software_stacks/ble_stack/icall_ble/icall_api_lite.o" "software_stacks/ble_stack/icall_ble/icall_hci_tl.o" "software_stacks/ble_stack/icall_ble/rd_ble_user_config.o" "software_stacks/ble_stack/profiles/devinfoservice.o" "software_stacks/ble_stack/profiles/gattservapp_util.o" "software_stacks/ble_stack/profiles/provisioning_gatt_profile.o" "software_stacks/ble_stack/profiles/remote_display_gatt_profile.o" "software_stacks/ble_stack/rosc/rcosc_calibration.o" "software_stacks/ti15_4stack/mac/hal/target/itm.o" "software_stacks/ti15_4stack/mac/high_level/mac_cfg.o" "software_stacks/ti15_4stack/mac/low_level/mac_activity.o" "software_stacks/ti15_4stack/mac/low_level/mac_settings.o" "software_stacks/ti15_4stack/mac/services/saddr.o" "software_stacks/ti15_4stack/osal_port/osal_port.o" 
    
    rm -rf "software_stacks/ti15_4stack/osal_port/osal_port_timers.o" "software_stacks/ti15_4stack/radio_configuration/mac_user_config.o" "software_stacks/ti15_4stack/stack_user_api/api_mac.o" "software_stacks/ti15_4stack/stack_user_api/macTask.o" 
    
    rm -rf "syscfg/ti_ble_config.d" "syscfg/ti_dmm_application_policy.d" "syscfg/ti_devices_config.d" "syscfg/ti_radio_config.d" "syscfg/ti_drivers_config.d" "OAD/bim_util.d" "OAD/crc32.d" "OAD/flash_interface_ext_rtos_NVS.d" "OAD/mark_switch_factory_img.d" "OAD/oad.d" "OAD/oad_image_header_app.d" "OAD/oad_util.d" "application/ble_remote_display/remote_display.d" "application/ble_remote_display/startup/ble_user_config_stack.d" "application/ble_remote_display/startup/osal_icall_ble.d" "application/ble_remote_display/startup/rom_init.d" "application/ble_remote_display/util/util.d" "application/cui/cui.d" "application/lpstk/adxl362/scif.d" "application/lpstk/adxl362/scif_framework.d" "application/lpstk/adxl362/scif_osal_tirtos.d" "application/lpstk/lpstk.d" "application/lpstk/lpstk_sensors.d" "application/main.d" "application/sensor/link_controller/jdllc.d" "application/sensor/sensor.d" "application/sensor/ssf.d" "application/sensor/util/mac_util.d" "application/sensor/util/util_timer.d" "dmm/application_policy/dmm_priority_ble_154sensor.d" 
    
    rm -rf "drivers/nv/crc.d" "drivers/nv/nvocmp.d" "sail/hdc2010.d" "sail/opt3001.d" "software_stacks/ble_stack/icall/icall.d" "software_stacks/ble_stack/icall/icall_cc2650.d" "software_stacks/ble_stack/icall/icall_user_config.d" "software_stacks/ble_stack/icall_ble/icall_api_lite.d" "software_stacks/ble_stack/icall_ble/icall_hci_tl.d" "software_stacks/ble_stack/icall_ble/rd_ble_user_config.d" "software_stacks/ble_stack/profiles/devinfoservice.d" "software_stacks/ble_stack/profiles/gattservapp_util.d" "software_stacks/ble_stack/profiles/provisioning_gatt_profile.d" "software_stacks/ble_stack/profiles/remote_display_gatt_profile.d" "software_stacks/ble_stack/rosc/rcosc_calibration.d" "software_stacks/ti15_4stack/mac/hal/target/itm.d" "software_stacks/ti15_4stack/mac/high_level/mac_cfg.d" "software_stacks/ti15_4stack/mac/low_level/mac_activity.d" "software_stacks/ti15_4stack/mac/low_level/mac_settings.d" "software_stacks/ti15_4stack/mac/services/saddr.d" "software_stacks/ti15_4stack/osal_port/osal_port.d" 
    
    rm -rf "software_stacks/ti15_4stack/osal_port/osal_port_timers.d" "software_stacks/ti15_4stack/radio_configuration/mac_user_config.d" "software_stacks/ti15_4stack/stack_user_api/api_mac.d" "software_stacks/ti15_4stack/stack_user_api/macTask.d" 
    
    rm -rf  "configPkg/" "syscfg/" 
    
    Finished clean
    
     
    
    **** Build Finished ****
    
    **** Build of configuration Release for project dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang ****
    
    /Applications/ti/ccs1120/ccs/utils/bin/gmake -k -j 9 all -O 
    
     
    
    Building file: "/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/apps/common/tirtos/ble_oad_lpstk_release.cfg"
    
    Invoking: XDCtools
    
    "/Applications/ti/xdctools_3_62_00_08_core/xs" --xdcpath="/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/.;/Applications/ti/xdctools_3_62_00_08_core/packages;/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source;/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/kernel/tirtos/packages;/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/kernel/tirtos7/packages;/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29;" xdc.tools.configuro -o configPkg -t ti.targets.arm.clang.M4F -p ti.platforms.simplelink:CC1352R1F3 -r release -c "/Applications/ti/ti_cgt_tiarmclang_1.3.0.LTS" --compileOptions "-march=thumbv7em -mcpu=cortex-m4 -mfloat-abi=hard -mfpu=fpv4-sp-d16 -mlittle-endian -mthumb -Oz -I\"/Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang\" -I\"/Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release\" -I\"/Applications/ti/ti_cgt_tiarmclang_1.3.0.LTS/include\" -I\"/Applications/ti/xdctools_3_62_00_08_core/packages\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/kernel/tirtos/packages\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/apps/\" -I\"/Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/application/sensor\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/common/boards\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/remote_display_profile_154\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/provisioning_profile\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/apps/common/ti154stack/source/ble_remote_display/app/\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/apps/common/ti154stack/source/ble_remote_display/\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/apps/dmm_154sensor_remote_display/source/\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/apps/sensor\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/common/cui\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/common\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/common/util\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/common/osal_port\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/common/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/fh\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/high_level\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/rom\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/inc/cc13xx\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/low_level/cc13xx\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/low_level/cc13xx/combo\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/tracer\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/hal/platform\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/hal/crypto\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/hal/rf\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/services/sdata\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ti154stack/services/saddr\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/common/cc26xx/npi/stack/\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/common/cc26xx/rcosc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/controller/cc26xx/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/rom\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/common/cc26xx\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/icall/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/hal/src/target/_common\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/hal/src/target/_common/cc26xx\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/hal/src/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/heapmgr\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/profiles/dev_info\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/profiles/simple_profile\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/icall/src/\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/icall/src/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack/osal/src/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/common/nv\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/common/cc26xx\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/ble5stack\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/posix/ticlang\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/devices/cc13x2_cc26x2\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/devices/cc13x2_cc26x2/inc\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/devices/cc13x2_cc26x2/rf_patches\" -I\"/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/devices/cc13x2_cc26x2/driverlib\" -DxFEATURE_ENHANCED_ACK -DCOMBO_MAC -DxUSE_ITM_DBG -DTIMAC_ROM_IMAGE_BUILD -DFLASH_ROM_BUILD -DLPSTK -DCC13XX -DCC13X2 -DCC13X2R1_LAUNCHXL -DDeviceFamily_CC13X2 -DSUPPORT_PHY_CUSTOM -DSUPPORT_PHY_50KBPS2GFSK -DSUPPORT_PHY_5KBPSSLLR -DSUPPORT_PHY_200KBPS2GFSK -DNVSSPI -DDMM_OAD -DSECURITY -gdwarf-3 -fshort-enums -munaligned-access -funsigned-char -fcommon -ffunction-sections -fdata-sections -march=armv7e-m  " "/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/source/ti/dmm/apps/common/tirtos/ble_oad_lpstk_release.cfg"
    
    Building file: "../dmm_154sensor_remote_display_oad_lpstk.syscfg"
    
    Invoking: SysConfig
    
    "/Applications/ti/ccs1120/ccs/utils/sysconfig_1.12.0/sysconfig_cli.sh" -s "/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29/.metadata/product.json" --script "/Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/dmm_154sensor_remote_display_oad_lpstk.syscfg" -o "syscfg" --compiler ticlang
    
    Running script...
    
    Validating...
    
    warning: CONFIG_GPIO_DRV(/ti/drivers/GPIO) gpioPin: Connected to hardware
    
    DIO23/2 is connected to DRV5055 Analog Output on the CC1352R1 LaunchPad. Consider selecting it in 'use hardware' above. Using a custom board?
    
    info: /ti/dmm/dmm applicationState0: Reserved for bitmask Any
    
    info: /ti/dmm/dmm numPolicies: The order of policy table entries matter to the DMM scheduler
    
    Generating Code (dmm_154sensor_remote_display_oad_lpstk.syscfg)...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_ble_config.h...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_ble_config.c...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_build_config.opt...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_ble_app_config.opt...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_154stack_config.h...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_154stack_features.h...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_dmm_application_policy.c...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_dmm_application_policy.h...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_dmm_custom_activities.h...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_devices_config.c...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_radio_config.c...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_radio_config.h...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_drivers_config.c...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_drivers_config.h...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_utils_build_linker.cmd.genlibs...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/syscfg_c.rov.xs...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_utils_runtime_model.gv...
    
    Writing /Users/munan/customer_apps/TTI/dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang/Release/syscfg/ti_utils_runtime_Makefile...
    
    0 error(s), 1 warning(s)
    
    Finished building: "../dmm_154sensor_remote_display_oad_lpstk.syscfg"
    
     
    
    making package.mak (because of package.bld) ...
    
    subdir_rules.mk:10: recipe for target 'build-342195601-inproc' failed
    
    js: "/Applications/ti/xdctools_3_62_00_08_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 139); 'linker.cmd' deleted.
    
    gmake[1]: *** [build-342195601-inproc] Error 1
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/linker.cmd'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: *** No rule to make target 'build-342195601', needed by 'configPkg/compiler.opt'.
    
    gmake: Target 'all' not remade because of errors.
    
    **** Build Finished ****

    Second build (without running a clean):

    **** Build of configuration Release for project dmm_154sensor_remote_display_oad_lpstk_app_CC1352R1_LAUNCHXL_tirtos_ticlang ****

    /Applications/ti/ccs1120/ccs/utils/bin/gmake -k -j 9 all -O 

     

    Building file: "/Applications/ti/simplelink_cc13xx_cc26xx_sdk_6_10_00_29...
     Code

    I built simple broadcaster as well just to sanity check, I still get the first round build errors but a second dirty build runs cleanly.

    Munan

  • Hi Munan,

    Thanks for the build log. I struggle to determine what your issue is. I have a suspicion that it is a mac only problem, I will need to get access to a mac machine to try to reproduce the issue.

    In the meantime, can you let me know if this is only a problem with the latest version of the SDK (v 6.10)?

    Regards,
    Nikolaj

  • Hi Munan,

    I haven't been able to get access to a mac machine, but it seems like this might be an issue for mac. I think your issue is also mentioned here: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1120554/cc1352p-unresolved-pincc26xx_hwattrs-symbol-from-some-library-file-what-now

    Would you be able to test this on a Windows machine, and see if you still get the same issue?

    Regards,
    Nikolaj

  • Hi Munan,

    This is a known issue:MacOS Monterey has compatibility issues with XDC Tools. For a workaround, please refer to the ticket EP-10721