This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R7: Wi-SUN embedded router node project with OAD

Part Number: CC1312R7


Hi, good day

I want to know if it is possible to port some of the OAD functionalities (external flash) found on the 15.4 stack for the WI-SUN embedded router-node project. If that's the case, which changes should be made to the flash parameters found, for example, in the linker file (.cmd)?

  • Hi Thiago,

    Unfortunately, we currently do not have OAD functionality support on WiSUN. Enabling OAD is not straight forward by only application level changes. But it is expected to be supported in the future.

    Regards,

    Sid