Hi
I've noticed some devices operate this chip outside the officially supported datasheet frequencies. I'm presuming they have done extended testing and within the operating voltage/temperature they are confident of the performance.
From my experiments, the risk here is that the chip may fail to lock the pll although I have seen some concerns that the output amplifier may be damaged outside these ranges.
Could someone from TI perhaps comment on the risks of unofficial operating frequencies?
I'm interested in a few things
- What are the risks if operating outside datasheet bands - can it cause damage or is it pll lock issues, frequency drift etc?
- If the pll doesn't lock correctly, does the device still apply power to the antenna (e.g. risk of transmitting way off band)
- What are the risks of antenna mismatch? If the antenna doesn't present a normal 50 ohm load (i.e. poor SWR) can the output amplifier be damaged and if so, whats an acceptable mismatch?
Many thanks