This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Can FL1 (BLM18HE152SN1D) and 6.8uH inductor be removed?

Part Number: CC1310

Hi team,

Here's an issue from the customer may need your help:

Can FL1 (BLM18HE152SN1D) and 6.8uH inductors be removed from the power circuit? If not, how to choose a smaller package?

Could you help check this case? Thanks.

Best Regards,

Cherry

  • Hi,

    The DCDC inductor can be removed; see app note https://www.ti.com/lit/swra640 chapter 11.

    Alternatively, a smaller 0603 footprint can also be used, Murata LQM18DN6R8M70L or TDK MLZ1608M6R8WT000.

    FL1 can be removed from the design but removing power filtering is always a compromise of the level of noise on the power. For a majority of applications this should not be needed.

    Best regards,

       Richard