Hi team,
Here's a question from the customer may need your help:
Relevant description can be found in section 5.4 Power consumption Summary of CC1310 Spec. This project uses electrical power, special AC/DC devices, and the customer has found the following info:
"Input voltage again rises above the UVLO rising threshold.
During this time the output voltage will be loaded by less than 100 NA."
Special Powered Rear AC/DC Component Output Voltage DC 3.6V, Quiescent current 89nA. After 250 seconds of power, VOUT3.6 V, and the current can reach 50mA.
What is the minimum required transient current for the CC1310 to start-up? Does the unfunctional IO need to be grounded?
VDDR has changed to 1.65V output in 250 seconds, are there any other modifications needed?
Thanks.
Best Regards,
Cherry