Other Parts Discussed in Thread: CC1352R
I would like to use cc1101 and PA for audio sender device that operates GFSK 200khz spectrum ( < 200kbps )
in the 606 – 614 MHz range.
1, Can the CC1101 function at these frequencies with the same power efficiency as the regular 433mhz etc bands with the correct front end tuning?
2, how do remove the padlock in Smart RF STDUDIO so I can enable these frequencies?
Is there a better transceiver part choice that can modulate 2 or 4 FSK / GFSK in the 606-614mhz range?
thanks in advance ,