Hi Texas Instruments
We are using a C1120 chip on a six-layer RF board that has the RF output feeding a 1 Watt PA Harmonic filter and Tx/Rx switch.
We configure the C1120 via SPI to Tx mode FSK and the chip generated FSK which was originally fed to the PA .
To identify/ isolate the problem the PA has been isolated with its own 3V3 power supply, The PA is currently ran in isolation with its own RF source.
. RF IN and Out soldered directly to the RF board IN/ Out
The C1120 output goes directly to a spectrum analyzer for display.
The PA input come directly from an external signal generator at 10 dBm . The PA output immediately after matching connects to an attenuator and then into a spectrum analyzer. The PA is about 3cm from the C1120. Ample plated through holes. Coplanar 50 ohms tracking. Separate ground planes
Problem sequence.
The PA is power up(RF OFF).
The C1120 micro is power up. The C1120 is set to Tx via SPI. The SPI EXCHANGE IS monitored on an oscilloscope.
The C1120 RF out is monitored on a spectrum analyzer.
As soon as the PA RF is turned on, the C1120 goes into Rx / idle mode ?. Out test frequency is 450MHz.
The C1120 RF output seems to turn off. The C1120 TRX_SW (Pin18) goes from Low to Hi indicating the C1120 has decide to go into Rx. The SPI commands are continued to be send, but the SPI MISO (Master In Slave Out) stops sending data and goes low- just stops.
My hypothesis is internally in the C1120 has a Sensitive RSSI Log amplifier that picks up the PA LEAKAGE RF and the C1120 decided it is going in to receive mode when RF leaks in to the C1120 internal log amp.
It is our probably unreasonably to expect sufficient isolation from a 1 watt PA with volts swing LEAKING in to the C1120 internal, since the chip is not really EMC/ EMC isolated. All the decoupling rules have been followed, buried ground plane with RF on one side and power and slow signal on the other / own side.
Each of the SPI line have a 10MHz filter.
We hope you can offer some discussion / conjecture on our theory that RF is LEAKING into C1120 internal log amplification and this result in a CHANGE of mode to receiver mode.
Let me know for more information is required? Sketch attached.
Look forward to any suggestions.
Cheers. Peter.