This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1201: LNA input impedance

Part Number: CC1201


Using the CC1201 without the PA, and driven from a 50 antenna what is the input

impedance of the LNA ports pins at 950 MHz? This info is in the CC13XX Hardware & PCB

ap note. Can someone confirm the LNAs are identical for these two parts? Is there a recommended

BALUN transformer or must one use discrete L&Cs.