This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1125: TX is not correct at 19200bps

Part Number: CC1125


Hi Team,

The mode I use is synchronous_ serial_ Mode: 9600bps air baud rate can be transmitted and transmitted normally, but 19200bps air baud rate can only be transmitted by RX, and TX is not correct. I use an oscilloscope to measure TX_ RX_ CLK waveform, found that the rate waveform is incorrect, TX_ The waveform of DATA is also wrong My configuration IOCFG3=0X08, IOCFG2=0X09, IOCFG1=0XB0, IOCFG0=0X309600bps and 19200bps switching is SYMBOL_ The RATE 1/2/3 is different from the frequency offset. Everything else is the same. Thank you.

Best Regards

James

  • This post doesn't contain enough information. It should be possible to re-create what you are seeing without follow-up questions. 

    - The  IOCFG settings is not relevant in this case.

    - Please provide register settings for both cases in table form

    - Please provide the oscilloscope measurements 

  • Hi TheGhostOf

     
    static const registerSetting_t registerSettings[]= 
    {
        {CC112X_IOCFG3, 0x08},
        {CC112X_IOCFG2, 0x09},
        {CC112X_IOCFG1, 0xB0},
        {CC112X_IOCFG0, 0x30},
        {CC112X_SYNC3,  0xCC},
        {CC112X_SYNC2,  0xCC},
        {CC112X_SYNC1,  0xCC},
        {CC112X_SYNC0,  0xCC},
        {CC112X_SYNC_CFG1, 0x0B},
        {CC112X_SYNC_CFG0, 0x17},
        {CC112X_DEVIATION_M, 0x70}, // Frequency Deviation 
        {CC112X_MODCFG_DEV_E, 0x0A},
        {CC112X_DCFILT_CFG,  0x56},
        {CC112X_PREAMBLE_CFG1, 0x00},
        {CC112X_PREAMBLE_CFG0, 0x35},
        {CC112X_FREQ_IF_CFG, 0x31},
        {CC112X_IQIC, 0xCE},
        {CC112X_CHAN_BW, 0x0D},// RX Filter BW 
        {CC112X_MDMCFG1, 0x06},
        //{CC112X_MDMCFG0, 0x0A}, //RX
        {CC112X_MDMCFG0, 0x05},  //TX
        {CC112X_SYMBOL_RATE2, 0x7F},
        {CC112X_SYMBOL_RATE1, 0x75},
        {CC112X_SYMBOL_RATE0, 0x10},
       // {CC112X_AGC_REF,      0x20},
        {CC112X_AGC_CS_THR, 0xEA},
        //{CC112X_AGC_CFG1, 0x0A}, //RX
        {CC112X_AGC_CFG1, 0x2D}, //TX
        {CC112X_AGC_CFG0, 0x5F},
        {CC112X_FIFO_CFG, 0x00},
        {CC112X_FS_CFG, 0x14},
        {CC112X_PKT_CFG2, 0x05},
        {CC112X_PKT_CFG1, 0x00},
        {CC112X_PKT_CFG0, 0x20},
        {CC112X_PA_CFG2, 0x5D},
        {CC112X_PA_CFG0, 0x7E},//PA = 0dBm
        {CC112X_IF_MIX_CFG, 0x00},
        {CC112X_FREQOFF_CFG, 0x22}, //rx
        //{CC112X_FREQOFF_CFG, 0x24}, //Tx
        {CC112X_FREQ2, 0x5A},
        {CC112X_FREQ1, 0x5F},
        {CC112X_FREQ0, 0x5C},
        {CC112X_IF_ADC0, 0x05},
        {CC112X_FS_DIG1, 0x00},
        {CC112X_FS_DIG0, 0x5F},
        {CC112X_FS_CAL0, 0x0E},
        {CC112X_FS_DIVTWO, 0x03},
        {CC112X_FS_DSM0, 0x33},
        {CC112X_FS_DVC0, 0x17},
        {CC112X_FS_PFD, 0x50},
        {CC112X_FS_PRE, 0x6E},
        {CC112X_FS_REG_DIV_CML, 0x14},
        {CC112X_FS_SPARE, 0xAC},
        {CC112X_XOSC5, 0x0E},
        {CC112X_XOSC3, 0xC7},
        {CC112X_XOSC1, 0x07},
        {CC112X_SERIAL_STATUS, 0x08},
    };
    void Init_CC112x_TX()
    {
           uint8_t writeByte;
          //Set serial mode specific registers
          writeByte = 0x08;
          cc112xSpiWriteReg(CC112X_IOCFG3, &writeByte, 1);
          writeByte = 0xb0;
          cc112xSpiWriteReg(CC112X_IOCFG2, &writeByte, 1);
          writeByte = 0x30;
          cc112xSpiWriteReg(CC112X_IOCFG0, &writeByte, 1);
          writeByte = 0x08;
          cc112xSpiWriteReg(CC112X_SYNC_CFG1, &writeByte, 1);
          writeByte = 0x00;
          cc112xSpiWriteReg(CC112X_PREAMBLE_CFG1, &writeByte, 1);
          writeByte = 0x06;
          cc112xSpiWriteReg(CC112X_MDMCFG1, &writeByte, 1);
          writeByte = 0x05;
          cc112xSpiWriteReg(CC112X_MDMCFG0, &writeByte, 1);
          writeByte = 0x2D;
          cc112xSpiWriteReg(CC112X_AGC_CFG1, &writeByte, 1);
          writeByte = 0x05;
          cc112xSpiWriteReg(CC112X_PKT_CFG2, &writeByte, 1);
          writeByte = 0x00;
          cc112xSpiWriteReg(CC112X_PKT_CFG1, &writeByte, 1);
          writeByte = 0x08;
          cc112xSpiWriteReg(CC112X_SERIAL_STATUS, &writeByte, 1);
          
    }
    void Init_CC112x_RX()
    {
          uint8_t writeByte;
          //Set serial mode specific registers
          writeByte = 0x08;
          cc112xSpiWriteReg(CC112X_IOCFG3, &writeByte, 1);
          writeByte = 0x09;
          cc112xSpiWriteReg(CC112X_IOCFG2, &writeByte, 1);
          writeByte = 0xb0;
          cc112xSpiWriteReg(CC112X_IOCFG0, &writeByte, 1);
          writeByte = 0x1F;
          cc112xSpiWriteReg(CC112X_SYNC_CFG1, &writeByte, 1);
          writeByte = 0x00;
          cc112xSpiWriteReg(CC112X_PREAMBLE_CFG1, &writeByte, 1);
          writeByte = 0x06;
          cc112xSpiWriteReg(CC112X_MDMCFG1, &writeByte, 1);
          writeByte = 0x0A;
          cc112xSpiWriteReg(CC112X_MDMCFG0, &writeByte, 1);
          writeByte = 0x0A;
          cc112xSpiWriteReg(CC112X_AGC_CFG1, &writeByte, 1);
          writeByte = 0x05;
          cc112xSpiWriteReg(CC112X_PKT_CFG2, &writeByte, 1);
          writeByte = 0x00;
          cc112xSpiWriteReg(CC112X_PKT_CFG1, &writeByte, 1);
          writeByte = 0x08;
          cc112xSpiWriteReg(CC112X_SERIAL_STATUS, &writeByte, 1);
    }
    void CC112x_19200()
    {
           uint8_t writeByte;
           
           writeByte = 0xA3; //4K
           cc112xSpiWriteReg(CC112X_DEVIATION_M, &writeByte, 1);
           writeByte = 0x0A;
           cc112xSpiWriteReg(CC112X_MODCFG_DEV_E, &writeByte, 1);
           
           writeByte = 0x4E; //IQ image compensation disabled 
           cc112xSpiWriteReg(CC112X_IQIC, &writeByte, 1);
           writeByte = 0x06; //CHAN_BW 41.7 20
           cc112xSpiWriteReg(CC112X_CHAN_BW, &writeByte, 1);
           
           writeByte = 0x7F; //19.2KHz
           cc112xSpiWriteReg(CC112X_SYMBOL_RATE2, &writeByte, 1);
           writeByte = 0x75;
           cc112xSpiWriteReg(CC112X_SYMBOL_RATE1, &writeByte, 1);
           writeByte = 0x10;
           cc112xSpiWriteReg(CC112X_SYMBOL_RATE0, &writeByte, 1);
           
    }
    void CC112x_9600()
    {
           uint8_t writeByte;
           
           writeByte = 0xF7; //2.4k
           cc112xSpiWriteReg(CC112X_DEVIATION_M, &writeByte, 1);
           writeByte = 0x09;
           cc112xSpiWriteReg(CC112X_MODCFG_DEV_E, &writeByte, 1);
           
           writeByte = 0xCE; //IQ image compensation disabled 
           cc112xSpiWriteReg(CC112X_IQIC, &writeByte, 1);
           writeByte = 0x0D; //CHAN_BW 19.2  20 
           cc112xSpiWriteReg(CC112X_CHAN_BW, &writeByte, 1);
           
           writeByte = 0x6F; //9.6KBPS
           cc112xSpiWriteReg(CC112X_SYMBOL_RATE2, &writeByte, 1);
           writeByte = 0x75;
           cc112xSpiWriteReg(CC112X_SYMBOL_RATE1, &writeByte, 1);
           writeByte = 0x10;
           cc112xSpiWriteReg(CC112X_SYMBOL_RATE0, &writeByte, 1);
           
    }
    
    void Air_Rate_Init() //
    {
    	Radio_Para.Wireless_Link_Rate = Memory_Content[2];
    	switch(Radio_Para.Wireless_Link_Rate)
    	{
    		case '4':
    		CC112x_19200();
    		break;
    		case '2':
    		CC112x_9600();
    		break;
    		default:
    		Radio_Para.Wireless_Link_Rate = '2';
    		CC112x_9600();;
    		break;		
    	}
    }
    void Exti_Init()
    {
       /* TRX_SCK*/
        GPIO_MODER(RADIO_TRX_CLK_PORT,RADIO_TRX_CLK_PIN,0);//PA8
        GPIO_Speed(RADIO_TRX_CLK_PORT,RADIO_TRX_CLK_PIN,3);//50MHz
        GPIO_Pull_Up_Down(RADIO_TRX_CLK_PORT,RADIO_TRX_CLK_PIN,0);
        
        SYSCFG_EXTILineConfig(0,8); 
        
        if(Radio_Para.Operating_Mode == '2')  //RX
        {
              Ex_NVIC_Config(0,8,1);//PA8 FALLING
        }
        else if(Radio_Para.Operating_Mode == '0') //TX
        {
             Ex_NVIC_Config(0,8,2);//PA8 RISE
        }
    
        NVIC_Init(0,2,EXTI9_5_IRQn,2);
    
    }
    void InitCC112x()
    { 
          uint8_t writeByte;
          trxSpiCmdStrobe(CC112X_SRES); // Reset radio
          for(uint16_t i = 0; i < (sizeof(registerSettings)/sizeof(registerSetting_t)); i++) 
          {
              writeByte =registerSettings[i].data;
              cc112xSpiWriteReg( registerSettings[i].addr, &writeByte, 1);
          }
          cc112xSpiReadReg(CC112X_IOCFG3, &writeByte, 1);
          if(writeByte !=registerSettings[0].data)while(1);
          trxSpiCmdStrobe(CC112X_SCAL); 
          //cc112xSpiReadReg(CC112X_PARTNUMBER, &writeByte, 1);
          //if(writeByte!=0x58)while(1);
    }
    
    void Init_Radio()//TX
    {
    	Init_Sys();
        InitCC112x();
        ManualCalibration();
        Air_Rate_Init();
    	Init_CC112x_TX();
        Exti_Init();
    }
    

  • Hi TheGhostOf:

          TRx_CLK is 330k and  TX_DATA no data