This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: VDDS 3.3V and VDDS2 1.8V

Part Number: CC1310
Other Parts Discussed in Thread: CC1311R3

We have developed a custom board using the CC1310RHB.

VDDS and VDDS_DCDC is connected to 3.3V.

VDDS2 is connected to 1.8V, but this raises the voltage on VDDS2 to 2.2V.

The datasheet does state that VDDS2 > 1.9V, if VDDS > 2.7V.

So is it not possible to use both 3.3V and 1.8V on the CC1310, or am I misunderstanding something ?