This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: FCC and RED CERTIFICATION

Part Number: CC1101


Hi,

are the FCC and RED certifications avaibale?

We need them for a new project.

Thanks

  • Hi,

    There is no modular FCC certification for CC1101 that can be re-used.

    The CC1101 reference design has been made to pass ETSI certification.

  • Hi,

    is it possible to receive tests or certification regarding ETSI CERTIFICATION for CC1101?

  • Hi,

    These should not be needed since the CC1101 has been tested on an EM when mounted onto a SmartRF evaluation board. These will not help you pass your ETSI certification in any way. You will need to certify your board at the test house in order to achieve ETSI certification.

    When we test our LaunchPads at a test house, it is normally sufficient with SmartRF studio software and the actual LaunchPad. If your test house is requesting this information, then you can loop me into the discussion.