Hi team,
Here's the request from the customer:
Customer uses the cc1310+sky65115 circuit officially recommended and the official gerber file of TI to print and test.
Issue 1. SmartRF Studio 7 receives a maximum signal strength of -21db.
Issue 2. Using frequency 470Mhz single-ended transceiver mode, the distance is only about 500 meters outside.
- Customer doesn’t know why the input signal SmartRF Studio 7 shows the strongest -21db, even if the 1db signal is directly injected into the cc1310 FR-N or FR-P pin through the signal line, the display signal is only -21db, the schematic diagram is as follows.

- Why is the CRC error even when the outdoor distance is very short, only 500 meters?
- Is the setting of 470M single-ended mode correct?
Indoor test condition (left receive, right transmit):
Transmit Signal Strength:
Received signal strength:
Outdoor test condition (about 872 meters, actual straight line distance is about 500 meters.):
Pcb board (Sheet thickness 0.8mm material FR-4) :
Customers have commonly used tools such as spectrometers and network analyzers, shielded boxes, etc. Where and how should they test and check?
They want to figure out the actual transmission distance before designing their own products
Could you help check this case? Thanks.
Best Regards,
Nick