This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: Unable to run UART2 example

Part Number: CC1312R
Other Parts Discussed in Thread: SYSCONFIG

Hi,

I unable to run the UART2 example project (uart2callback_CC1312R1_LAUNCHXL_tirtos7_iar.eww)

IAR 5.50.9

SDK : simplelink_cc13xx_cc26xx_sdk_6_20_00_29

I got : 

  • Hi Yaki, 

    a. Is your Custom argument variables defined correctly, with path to sysconfig? 

    b. If it is defined correctly, can you please try opening a new workspace and try a clean build. Also, if it doesn't work please try it with a different device so that we know that no modifications are done to the EWP file of the project before building.

    Regards,

    Sid