Part Number: CC2652
Hi,
I'm working on a project with IMU (accelerometer) and MCU and we need to send this data wirelessly to a gateway and then to our server. For this project we start using Zigbee ( CC2652 ) but after checking some client's requeriments we think maybe it can't be enough because it implies to use several gateways ( concentrator with another CC2652 ) and try to synchronize them...
There is some other wireless technology to run +200 sensors on a wireless network with low bandwidth, low power, and long range (>100m) and, preferably, with only one gateway? Maybe using custom SubGHz implementation?
Because sensors needs to be low power, and it implies sleeping modes, maybe mesh is not feasible in this scenario, but at the end, no matter what (with intermediate concentrators or some other way), we need more than 100m coverage from base.
Greatings