This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LPSTK-CC1352R: LPSTK cc1352R

Part Number: LPSTK-CC1352R
Other Parts Discussed in Thread: CC1352P, CC1352R,

Hi Folks 

we are working on a health monitor for cattle using LPSTKcc1352R as transmitter and CC1352P as collector...

1.The expected range is 1 km ,but the current range which is getting is only 200mtrs

2.The battery life expectancy is of 2 years ,but the device is taking 3ma which will not go beyond 50 days(since we are using 3600mAh battery)

3.we are expecting minimum 200 nodes(sensors) in the network and which should auto connect when it comes to the range..

kindly suggest us a best solution for our project...

the SDK we are using is in LPSTK-DMM 15.4 remote OAD

and in collector-collector SDK from DMM

Thanks in advance