Other Parts Discussed in Thread: TMDSEMU110-U, TM4C129ENCZAD, AWR1843, AWR1843BOOST
Hello TI engineers.
I would like to ask the following questions first
① It is necessary to connect from the LAUNCHXL-1350's XDS110 connector to the 20-pin JTAG connector.
I have a JTAG wiring on a custom board with CTI-20 pins.
(Connector used is FTR-110-03-G-D-06)
Do you have a connector that can convert from 10 pins to 20 pins?
(2) If you come to the conclusion that the question in (1) is not true, is it okay to connect the necessary jumper wires yourself?
(Is it OK to connect only nRESET, TCK, TDI, TDO, and TMS at this time?
The Vtref pin supplies 3.3 V power to the target on the custom board without being tied to a power supply. )