This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC1352P7: Application question

Part Number: LP-CC1352P7
Other Parts Discussed in Thread: LPSTK-CC1352R, CC2650STK, CC2650

Hi Team,

Can you please help with the inquiry below?

1) Can the LP-CC1352P7-4 communicate with LPSTK-CC1352R in the 433 MHz range? Also, can the launchpad + STK pair be used for exhibiting the following networking protocols features:- Bluetooth LE support, Bluetooth mesh, Zigbee coordinator, zigbee network processor. 
2) Can the LP-CC1352P7-4 be programmed to act as a Zigbee coordinator and Zigbee network processor?
3) Can the LP-CC1352P7-4 communicate with CC2650STK. If yes, then using which protocols apart from BLE 5.1 can they communicate with?
The description & features on the product page of CC2650STK says "Additionally, the SensorTag can be enabled with ZigBee®/6LoWPAN technology."  So dos the CC2650STK support bidirectional communication using Zigbee and 6LoWPAN with LP-CC1352P7-4  ?

Thanks in advance.

Regards,

Marvin