Hello,
In using the CHIP lock-app example for the LP-CC2652R7, it seems as though using the SPI_transfer() function in slave-mode will lock up the board if a timeout is not specified. Is this expected?
In the example below, if params.transferTimeout = x; is not specified, the board appears to hang - i.e. there is no output on the serial debug.
Note that no data is being transferred over the SPI bus at the time:
void SpiSlaveTask(void * pvParameter)