This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Creating a third SPI interface on CC1310 RHB using DIO ports

Part Number: CC1310

Hi Experts,

We need your assistance with creating a third SPI interface on CC1310 RHB using DIO ports. Would this be possible?

When adding a third SPI mapping to configuration files, do we need to change SPI DMA parts in the cc1310_launchxl.c file? As far as I checked, if we do not add the third one, the initialization of SPI will fail and the system will just hang. If we are adding the new one, how should we define the following properties for the new SPI master?

 Thank you in advance for your support.

Best Regards,

Jonathan