Hi Team,
I would like to know if the DIO port of CC1310 can be configured as an SPI CLK. The requirement is to set-up a periodic timer with GPTimer0A and set the loadVal to 4 to have a frequency of 4MHz. However, the output can only generate 50kHz at most.
Is this caused by the extra time of interrupt and callback? Or the timer is not setup correctly? Is it even possible for CC1310 to toggle the port at such a high frequency?
Thank you kindly,
Regards,
Marvin