This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: CC1310 with WMBUS - Help with starting a new project

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: WMBUS, CC1310

Hello forum

I want to create a wmbus application that can handle t1 and c1 modes on the cc1310 launchpad. I Have seen the stackforce implementation of the wmbus stack but i have heard to stay away from it.

Is there any other modules that can be used?

Is there any modules in the project explorer that can setup the radio config running 868MHz and maybe a example module of wmbus running?