Hi,
So if we disable sleepy in syscfg on the sensor application, and try to do OAD from host_collector we get a DATA ACCESS exception in a HWI.
The problem is 100% repeatable. Every OAD attempt results in an exception.
Running *with* sleepy (CONFIG_RX_ON_IDL *unset*) works perfectly, 100%
I've set a breakpoint on the OAD message processing, and stepped through the code. Everything looks ok there.
I suspect there is an error in the MAC level of the stack. Is there a fix or workaround available?