This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Proprietary modulation

Part Number: CC1310


I am thinking of using this device in an industrial remote control application. 

It needs to be able to send two types of telegram.  The first is secure, encrypted in some way and if this takes a couple of hundred ms that is not a problem.  After the controlled device has acknowledge the first transmission I need to be able to send a lightweight shot telegram which is essentially a "keep doing that" message. 

If the controlled device misses a couple of these shorter transmission then it will stop what it is doing and won't start until it gets a new encrypted message.  The lightweight telegrams must be short and sent frequently, say every 20ms. 

What I am wondering therefore is will I be able to do this with the CC1310?

Marc Isherwood