I want to decode ADS-B, which uses Pulse Position Modulation at 1 mbaud. For PPM a 0 is OOK of 01, and a 1 is 10
In theory, the radio could match a preamble, decode OOK or ASK at 2 mbaud, and then let the MCU decode the PPM from bits. The CC1311 or CC1352 has the frequency and data rates to support ADS-B.
Is this possible?
Is there a different chip that would be better?
If it matters, the volume is roughly thousands a year.
Thanks