This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: what are possible causes for extremely low RSSI between radios that are in line of sight and only a few feet away?

Part Number: CC1310


Hi,

We deployed a network of radios based on TI-15.4 stack into a presumably quite noisy environment. The network consists of one collector radio, and 6 sensor nodes. They are about 4 ~ 10 feet away from each other and in line of sight. TX power for all radios are set a 7dBm.

So far communication between sensor nodes and the collector node seems quite reliably. But I am puzzled by the fact that RSSI as seen by both all sensor nodes and collector node are extremely low, vary between -115 and -100, average at -106 dBm. In our other similar deployments, the typical RSSI are between -70dBm and -30dBm.

What could be such low RSSI? Ideally we need to do something about it. Please advise.

Thanks,

ZL