This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC110L: CC110L drop-in compatibility vs CC1101

Part Number: CC110L
Other Parts Discussed in Thread: CC1101,

Hi,

I'm struggling to tell what the key differences are between the CC1101 and CC110L transceiver ICs. With regard to the attached schematic (which was designed for, and currently operates well with, the CC1101), is it possible to confirm whether the CC110L would work as a drop-in replacement? The 433MHz band is being used, with GFSK modulation. I'm essentially trying to work out if this design was done without knowledge of the cheaper option, or if there is a specific required functionality that is unique to the CC1101. 

Schematic:

/resized-image/__size/2560x960/__key/communityserver-discussions-components-files/156/radioSchem.png

Thank you.