This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC1352P7: Modification of Py-Spinel Code to handle the incoming UDP packets from Router node

Part Number: LP-CC1352P7

Dear Team,

Greeting of the day!

We will push the UDP data packets from Router Node (RN) to Border router (BR).

Basic use case : Creating a virtual tunnel between BR & RN to transfer sensor data as UDP Packets, this data is send periodically by RN on it's own as Unsolicited message to BR(* means BR will not send any request).

Our sensor sends the data over the UART interface periodically as a ASCII string, so we will basically send this data transparently to BR directly over a specific IP/Port. 

I have the following queries:

1. If we want is to monitor this data (Sensor ASCII string) at host side (*PC/Laptop) using the Py-Spinel interface connected to BR, from where I should start and where exactly I should make changes at BR code & spinel code to send or receive these Unsolicited message in the Py-spinel interface.

2. Can I bridge this data to the network, Like running a parallel application in the PC/Laptop and sending the received data to our server

Let me know if you need more details.

Thanks & Regards,

Harinder Singh