This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LPSTK-CC1352R: Dual Mode Tx and Rx

Part Number: LPSTK-CC1352R
Other Parts Discussed in Thread: CC1352R

Hi Experts,

Currently, i am working with CC1352R Custom board, now i am trying to send the data through BLE and Sub 1 Ghz so i just check the Dual mode TX/RX example, In both syscfg files have multiple selections on RF and BLE, i can't understand why the example have a multiple selections like 50kbps,200kbps,5kbps in RF and 100kbps, 200kbps in BLE,

I wonder to know so i just search for it, finally, i found this link

SysConfig Migration — SimpleLinkTm CC13x2 / CC26x2 SDK Proprietary RF User's Guide 3.30.00 documentation

it shows Migration, here i have a doubt 

1. In default RF transmits data through which setting 50kbps or 200kbps or 5kbps??

2. Is it possible to receive RF data alone if i use the RF packet RX example at 5kbps?? 

3. Is it possible to choose each one setting for BLE and RF??

4. If i want to choose 2.5kbps what i need to do in syscfg??

regards

Surya