This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1201: SmartRF Studio 7 Parameters Setup

Part Number: CC1201


Hi,

I am working on a project with CC1201 to receive signal with frequency range 430-470MHz, 12.5kHz channel spacing and data rate is 512bps. I have my custom board for this project, not the evaluation board. 

I am not sure how to set it up with the parameters I had above. From what I researched, the SmartRF Studio can be used to generate register values. I was tried to learn it online, but it is still very confusing after a few hours study. Especially the RX filter BW and deviation values. Anyone could help me with these? 

Thanks in advance.