Hello,
Is it possible to program/flash/erase/verify a CC1352R with a ST-Link (V3PWR, V3MINIE, V3MINI...) ? Or does it only work with Elptronic, XDS110, XDS200...
BR Sebastian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is it possible to program/flash/erase/verify a CC1352R with a ST-Link (V3PWR, V3MINIE, V3MINI...) ? Or does it only work with Elptronic, XDS110, XDS200...
BR Sebastian
Hi Sebastian,
You could technically use the ST-Link UART pins to program the device flash using the CC1352R built-in serial bootloader, but I would not recommend it.
Instead, it would indeed be better for you to acquire an XDS110.
Regards,
Arthur
Ok. Understand. One more question: with the STLink SWD mode it's also not possible? Are SWD and cJTAG compatible?
Hi Sebastian,
cJTAG and SWD are different protocols.
The CC1352r does not support SWD.
Regards,
Arthur
The CC2642 being the same family as the CC1352, it does not support SWD either indeed.
Our newest device, CC2340Rx does uses SWD as its debug interface: https://www.ti.com/product/CC2340R5
Regards,
Arthur
Sebastian,
I do not think so, and this is not something that we will test.
You could have however have a look at openocd/black magic debuggers, but as far as I know, as of today, none of them support the CC2340.
Regards,
Arthur