Hi team,
Here's the request from the customer:
All other peripherals are turned off, and the chip consumes 3.7mA when run while(1)?
The board is customer board and there are only about 2 ua when the chip sleep. The 24M in the datasheet is only 1.9 mA, which is not the same as the actual measurement.
Following is the package of customer's program:7801.demo.zip
Could you help check this case? Thanks.
Best Regards,
Nick